Technical FAQs

Ask a Question

Can you put in a blank main breaker kit to take up the space in a MH74 if you have a NQOD454L400 interior which ordinarily would take a MH62 can?

A blank main breaker kit can be added in the MH74 can if you have a NQOD454L400 interior which ordinarily would take a MH62 can.
OR
12`` rail and deadfront extensions can be installed at the mains end of the panel. Part numbers are as follows:

(1) 80120-823-04 (12`` left rail ext.)
(1) 80120-824-04 (12`` right rail ext.)
(1) 80110-876-04 (12`` deadfront ext.)
(4) 21590-17081 (Rail ext. screws)

Revised 3/10/04



CTA-ID : 2000606
Was this helpful?
What can we do to improve the information ?