Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DU322 General Duty Safety Switch?

Issue:
Product Design Features

Product Line:
General Duty Safety Switches

Environment:
Terminal lug data

Cause:
Application

Resolution:

The terminal lug data per the NEC wire bending space is (1) #10 - 3 AWG aluminum or #14 - 3 AWG copper conductors per phase. The lugs that come in the switch, will actually accept (1) #2 AWG MAX conductors, BUT the wire bending space available in the switch restricts the maximum to #3 AWG conductors.


CTA-ID : 2001361
Was this helpful?
What can we do to improve the information ?