Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DU323 General Duty Safety Switch?

The lugs on this device will accept (1) #12 - 1/0 AWG aluminum or #14 - 1/0 AWG copper conductors per phase. Although the lug will accept #1/0 AWG conductors, the wire bending space available in the switch restricts the maximum to #1 AWG conductors.


CTA-ID : 2001354
Was this helpful?
What can we do to improve the information ?