Technical FAQs

Ask a Question

Can a QOM2225VH be installed in a QO140M200 load center to upgrade it to 225 ampere?

No, the load center is marked for 200 ampere maximum. Installing a QOM2225VH would violate the listing and labeling of the device. Consider a QO140M225 for this application.

CTA-ID : 2001102
Was this helpful?
What can we do to improve the information ?