Technical FAQs

Ask a Question

How many characters per line and lines will go onto the 9001KXN199 legend plates?

In 1/4 in letters it is 7 characters and 4 lines, with 3-16 letters it is 9 characters and 5 lines and with 1/8 in characters it is 14 characters and 8 lines.




CTA-ID : 2000870
Was this helpful?
What can we do to improve the information ?