Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DU324 General Duty Safety Switch?

Issue:
Product Design Features

Product Line:
General Duty Safety Switches

Environment:
Lug data

Cause:
Installation

Resolution:

The NEC wire bending space in this switch is ONLY for (1) #6 - 250kcmil Al or CU wire per Phase. But the Lugs that are used in the switch will accept (1) #6 - 300kcmil wire. 



 
Was this helpful?
What can we do to improve the information ?