Technical FAQs

Ask a Question

What is the Terminal Lug Data for a 92251, Series T4, Double Throw Safety Switch?

Issue:
Product features

Product Line:
Double Throw Safety Switch

Environment:
lug data

Cause:
installation

Resolution:
The lugs on this device will accept (1) #12 - 8 AWG aluminum or #14 - 8 AWG copper conductors per phase.

 
Was this helpful?
What can we do to improve the information ?