Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DTU362DS Double Throw Safety Switch?

Issue:
Product features

Product Line:
Double Throw Safety Switches

Environment:
Wire size

Cause:
installation

Resolution:
The lugs on this device will accept (1) #12 - #2 AWG Aluminum wire OR (1) #14 - #2 AWG copper wire per phase.

 
Was this helpful?
What can we do to improve the information ?