Technical FAQs

Ask a Question

Can the current style I-Line trim door kits used with four-piece trims be used with four-piece trims supplied before 8/97?

No. The current ``door kit`` will not fit the older style four-piece trims.
Customer would need to order a complete current style, 4 piece trim with the door.



CTA-ID : 2001075
Was this helpful?
What can we do to improve the information ?