Technical FAQs

Ask a Question

Will a HOM30M200C load center accept a HOMT Tandem or HOMT Quad Tandem circuit breaker?

Issue:
Product Feature

Product Line:
HOM LC

Cause:
Understanding if HOMT breakers can be used

Resolution:
No, it will not. This is a 30 space/30 circuit panel, accepting ONLY full size HOM branch breakers only.


CTA-ID : 2001069
Was this helpful?
What can we do to improve the information ?