Technical FAQs

Ask a Question

Can an SDSB1175C be used with a Homeline panel?

The SDSB1175C can be used with any 120/240Vac, single phase load center. The warranty terms are better if used with a Square D QO or Homeline load center.


CTA-ID : 2000840
Was this helpful?
What can we do to improve the information ?