Technical FAQs

Ask a Question

Can an NQOD panel be used on a 240V 3PH 3W Delta system?


Issue:
System application

Product Line:
Panelboards

Environment:
NQOD

Cause:
240v 3PH app

Resolution:
Yes. Branch breakers must be 3P or QO--H / QOB--H and must carry a full 240V rating.

NOTE: This is not the same as a 240D/120VAC 3PH 4W system.




 
Was this helpful?
What can we do to improve the information ?