Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DTU222 Double Throw Safety Switch and are there alternate lugs?

Issue:
Product Design features

Product Line:
Double Throw Safety Switches

Environment:
Lug wire size

Cause:
Installation

Resolution:
The lugs on this device will accept (1) #12 - 2 AWG aluminum or #14 - 2 copper conductors per phase.

The Only alternate lugs are Compression lugs(see wiring diagram or current digest), BUT the wire size and quantity remains the same

 
Was this helpful?
What can we do to improve the information ?