Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DT323 Double Throw Safety Switch?

The lugs on this device will accept (1) #12 - 1/0 AWG aluminum or #14 - 1/0 AWG copper conductors per phase.


CTA-ID : 2001286
Was this helpful?
What can we do to improve the information ?