Technical FAQs

Ask a Question

What class of fuse will the QMB324W accept?

Issue:
Product design features

Product Line:
Heavy Duty Safety Switches

Environment:
Fuses

Cause:
Installation

Resolution:

These switches accept Class H or K fuses as standard. Options include Class R fuses (field install Class R Fuse Kit HRK1020) With Class H or K fuses installed, the switches are UL listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R fuses (and Class R Fuse Kit HRK1020 installed, the switches are UL listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.
This switch is for use with Class H or R.

NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.

CTA-ID : 2001291
Was this helpful?
What can we do to improve the information ?