Technical FAQs

Ask a Question

What is the Terminal Lug Data for a 92351, Series E, Double Throw Safety Switch?

The lugs on this device will accept (1) #12 - 2 AWG aluminum or #14 - 2 AWG copper conductors per phase. However, the wire bending space provided restricts the conductors to a #3 AWG maximum.


CTA-ID : 2001280
Was this helpful?
What can we do to improve the information ?