Technical FAQs

Ask a Question

What lugs are used for the EZM11200CBU Main Device?

Product Design Features

EZ Meter-Pak Metering Equipment

Terminal Lug Data


The EZM11200CBU does not have line side lugs provided. The suffix "U" of the catalog number indicates that the device meets EUSERC standards. EUSERC requires factory supplied lug landing pads to accept field installed lugs. In EUSERC locations, the lugs will normally be supplied by the Utility Company. For contractor supplied lugs, the lugs should be ordered separately. Lugs listed for use on this device will be noted on the devices wiring diagram (located inside the front cover). You may also refer to the below attached CAD Drawing #3116 or Catalog 4100CT9801 for a list of acceptable lugs. The referenced Catalog and CAD Drawing are accessible via the Internet on

CTA-ID : 2001052
Was this helpful?
What can we do to improve the information ?