Technical FAQs

Ask a Question

What is the voltage rating of an HU362, HU362RB, HU362DS, HU362A or HU362AWK safety switch?

Issue:
Application

Product Line:
HD SS

Cause:
Clarification of voltage rating

Resolution:
These switches are rated for 600Vac or 600Vdc maximum.


CTA-ID : 2001042
Was this helpful?
What can we do to improve the information ?