Technical FAQs

Ask a Question

Does Square D offer a pedestal extension for the UHTRP242363 meter socket?

Issue:
Product design features

Product Line:
Individual Meter Sockets

Environment:
Accessory

Cause:
Application

Resolution:
Yes, use part number 1007680. This is an 18" extension piece


CTA-ID : 2000778
Was this helpful?
What can we do to improve the information ?