Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DU222RB General Duty Safety Switch?

The lugs on this device will accept (1) #10 - 2 AWG aluminum or #14 - 2 AWG copper conductors per phase. Although the lug will accept #2 AWG conductors, the wire bending space available in the switch restricts the maximum to #3 AWG conductors.


CTA-ID : 2001506
Was this helpful?
What can we do to improve the information ?