Technical FAQs

Ask a Question

What is the Terminal Lug Data for a L211N Light Duty safety switch?

The lugs on this device will accept (1) #14 - 6 AWG copper or (1) #12 - 6 AWG aluminum conductors per phase. However, wire bending space provided in the switch restricts the conductors to #8 AWG maximum.


CTA-ID : 2001503
Was this helpful?
What can we do to improve the information ?