Technical FAQs

Ask a Question

How much force does it take to toggle the handle of an EDB, EGB or EJB breaker?

For 15 - 30A
From Off to On it takes 8 lbs of force
From On to Off it takes 4 lbs of force
From trip to reset it takes 7 lbs of force

For 35 - 70A
From Off to On it takes 10 lbs of force
From On to Off it takes 4.5 lbs of force
From trip to reset it takes 9 lbs of force <>

For 80 - 125A
From Off to On it takes 14 lbs of force
From On to Off it takes 6.5 lbs of force
From trip to reset it takes 11 lbs of force


CTA-ID : 2001499
Was this helpful?
What can we do to improve the information ?