Technical FAQs

Ask a Question

Can a door Lock Kit be added to the cover used on the QO130M200 load center?

Issue:
product features

Product Line:
QO load centers

Resolution:

Yes, use the PK6FL lock kit. Two keys are provided with the PK6FL. A replacement key is also available, catalog number LP9618.


CTA-ID : 2000183
Was this helpful?
What can we do to improve the information ?