Technical FAQs

Ask a Question

Will a HOM3040M200RB load center accept a HOMT tandem or quad tandem circuit breaker?

Yes, this is a 30 space/40 circuit panel, accepting a maximum of (10) HOMT tandem or (4) HOMT quad tandem circuit breakers.


CTA-ID : 2002259
Was this helpful?
What can we do to improve the information ?