Technical FAQs

Ask a Question

What is the bar graph between the two .5 delay settings on standard function Micrologic trip units?

Any setting between the two .5`s is still a .5 setting. The same physical switch is used on standard and full function tripunits. The full function trip unit uses more switch settings than the standard trip unit. Therefore, duplicate numbers are used to fill in unused switch settings.

CTA-ID : 2000174
Was this helpful?
What can we do to improve the information ?