Technical FAQs

Ask a Question

What is the function of an arc suppressor?

When a switch is opened under load, an arc develops as the switch blades are separated from the switch jaws. The Arc Suppressors helps to dissipate the arc and prevents the arc from crossing between phases or from phase to ground.


CTA-ID : 16100
Was this helpful?
What can we do to improve the information ?