Technical FAQs

Ask a Question

What is the catalog number and availability for a Trilliant branch breaker, 2 pole, 100 ampere.

The catalog number is SDT2100. This breaker is obsolete and no longer available. The only alternative is to purchase a complete 100 ampere Main Breaker Interior, SDTN20M100. The SDT2100 provided with this interior can be used as a branch breaker on 150 and 200 ampere mains Trilliant panels.

CTA-ID : 12481
Was this helpful?
What can we do to improve the information ?