Technical FAQs

Ask a Question

What is the catalog number for a trim clamp that has a gray plastic washer-like part in front with a slot head screw through its center, and in back a mechanism similar in appearance to half of an old-fashioned spring clothespin?

LP9501, used on I-Line series 1 panelboards, NEHB 600A Series E1, and NQOD 400A and 600A Series E1 trims.


CTA-ID : 2000162
Was this helpful?
What can we do to improve the information ?