Technical FAQs

Ask a Question

Can a 125amp Main Circuit breaker be obtained for the QO342M150 Load center?

Issue:
Product Design Features

Product Line:
QO Three Phase Load Centers

Environment:
Main Breaker

Cause:
Application

Resolution:

NO, The QO342M150 is an older series load center that used the KDL32150 type main breaker and these main breakers are Obsolete, No Longer available,with no replacement. 


CTA-ID : 2000159
Was this helpful?
What can we do to improve the information ?