Technical FAQs

Ask a Question

Can the ATV28 drive be started by remote start signal if the local operator kit is installed?

Issue:   Can the ATV28 drive be started by remote start signal if the local operator kit is installed?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   
No. The drive can only be started by means of the start button on the potentiometer kit once that kit is installed.


 
Was this helpful?
What can we do to improve the information ?