Technical FAQs

Ask a Question

Do they XUDJ/ XUDH amplifier devices come with fiber optic cables? <br />

No. The end user will need to order the glass fiber optics XUFS or plastic XUFN type cable separate from the amplifier. See Digest 172, pg. 17-23.


CTA-ID : 16085
Was this helpful?
What can we do to improve the information ?