Technical FAQs

Ask a Question

What is the maximum short circuit current rating that can be achieved with a Homeline load center?

Generally, Fixed Main Lugs devices are rated 10,000 AIR. Convertible Main Lugs and Universal Mains devices are rated 10, 000 AIR, with a 22,000/10,000 AIR Series rating available by field installing a QOM1-VH or QOM2-VH Main Breaker. Convertible Main Breaker devices are rated for 22,000 AIR.

CTA-ID : 16078
Was this helpful?
What can we do to improve the information ?