Technical FAQs

Ask a Question

What field installable pilot light kit for an 8536 size 2 starter can be used for 240V?

Class 9999 Type SP3R pilot light kit comes standard with a red lens and is powered by an thin wafer looking induction coil, which when installed onto the starter coil, induces approximately 6VAC to power the light. It makes no difference what the operating voltage of the coil is because the induced voltage will always be the same. The magnetic lines of flux around the coil core induces the voltage onto the pilot light induction coil.


CTA-ID : 2000469
Was this helpful?
What can we do to improve the information ?