Technical FAQs

Ask a Question

Where is the best place to mount a HOM2175SB Secondary Surge Arrestor in a HOMELINE load center?

The HOM2175SB can be mounted anywhere in the HOMELINE panel, but ideally should be located as close to the Mains as possible. The neutral conductor should be routed and connected to the panels neutral assembly in the shortest distance possible. Cut the neutral wire to the shortest length possible to reach and connect to the panels neutral assembly, for the best protection.


CTA-ID : 2000459
Was this helpful?
What can we do to improve the information ?