Technical FAQs

Ask a Question

Can more than one QO Distribution Panel (i.e. HQO__ style) be installed into a 240 volt HCN I-lIne panelboard ?

Yes, the only restriction is the 4.5`` of mounting space required by each unit.
If the I-Line is being used as a lighting and appliance panelboard, it must not exceed the 42ckt rule.


CTA-ID : 2000145
Was this helpful?
What can we do to improve the information ?