Technical FAQs

Ask a Question

Are NEMA 1 enclosures offered for encapsulated transformers for indoor applications?

An encapsulated transformer is offered with a standard NEMA 3R rated enclosure which is suitable for both indoor and outdoor applications.


CTA-ID : 2000141
Was this helpful?
What can we do to improve the information ?