Technical FAQs

Ask a Question

What is the part number for the heatsink fan and door fan on the Omegapak 8804 CT (1-40hp @ 460 VAC), EVT & VT (1-50hp @ 460 VAC) ?

The part number is 26016-31450 which can be used as a Door or heat sink fan


CTA-ID : 4136
Was this helpful?
What can we do to improve the information ?