Technical FAQs

Ask a Question

Does Square D offer low voltage dry type transformers built to ABS or American Boat Yacht Council standards?

Square D builds and tests low voltage dry type to all applicable ANSI, NEMA and UL standards. We do not test to either ABS or ABYC standards.


CTA-ID : 2000132
Was this helpful?
What can we do to improve the information ?