Technical FAQs

Ask a Question

What is IDMTL?

IDMTL is the Inverse Definite Minimum Time Lag. It is a function that allows changing the slope of the long time delay trip curve and is used for system coordination. The trip time can never exceed the tr=24 second I2t time-current curve.

This feature is only available on Micrologic Power and Harmonic trip units for the P-frame, R-frame, and Masterpact breakers.

CTA-ID : 2000127
Was this helpful?
What can we do to improve the information ?