Technical FAQs

Ask a Question

Are MAL circuit breakers 100% rated?

No. The ME and MEL are, but Square D thermal-magnetic breakers must be derated to 80% for continuous loads.


CTA-ID : 2000119
Was this helpful?
What can we do to improve the information ?