Technical FAQs

Ask a Question

What type of hubs are used with the MP43200 Meter-Pak?

Product Line:
MP Meter-Pak

Environment:
Metering

Cause:
Need hub to bring conduit into an MP Meter-Pak

Resolution:
This Meter-Pak's utility compartment will accept two A-L type hubs (2" through 4") in the top endwall. Two closing plates, part number ACPL, are factory installed on the top endwall so the Meter-Pak can also be used for a bottom cable entry application. The bottom endwall will also accept two A-L type hubs (2" through 4"). The catalog numbers of the Series 'A-L' hubs are as follows;

2.0 inch - A200L
2.5 inch - A250L
3.0 inch - A300L
3.5 inch - A350L
4.0 inch - A400L 
Was this helpful?
What can we do to improve the information ?