Technical FAQs

Ask a Question

What type of hubs are used with the MPH55125 Meter-Pak?

This Meter-Paks` utility compartment will accept two A-L type hubs (2`` through 4``) in the top endwall. Closing Plates, ACPL, are factory installed on the top endwall for a bottom cable entry application. The bottom endwall will also accept two A-L type hubs (2`` through 4``).


CTA-ID : 16059
Was this helpful?
What can we do to improve the information ?