Technical FAQs

Ask a Question

What are the different NEMA types of enclosures available for the HOMELINE load centers?

Issue:
Product enclosure types

Product Line:
Homeline load centers

Environment:
NEMA ratings

Cause:
Application

Resolution:

The HOMELINE load centers are available ONLY in Nema type 1(Indoor) and Nema type 3R(Outdoor) enclosures.


CTA-ID : 2000434
Was this helpful?
What can we do to improve the information ?