Technical FAQs

Ask a Question

Are the MG24439 and MG17414 24vdc rated ?

Yes.... the UL1077 C60N breakers are rated up to 65vdc for a one pole, 125vdc for a two pole. The UL489A one pole to 60vdc max.


CTA-ID : 2000431
Was this helpful?
What can we do to improve the information ?