Technical FAQs

Ask a Question

Are alternate lugs available for a D224NRB safety switch to accommodate (2) conductors per phase?

This device is UL listed with the standard lugs supplied, which accommodate (1) #4 AWG - 250 kcmil Al/Cu conductors per phase. Alternate lugs have not been tested nor listed for use on the switch, so therefore cannot be recommended.

CTA-ID : 15740
Was this helpful?
What can we do to improve the information ?