Technical FAQs

Ask a Question

What type of hubs are used to feed a MP44125 Meter-Pak?

TOP Endwall will accept one Series A-L Hub and is supplied with one factory installed ACPL closing plate.
BOTTOM Endwall will accept two Series A-L Hubs or knockouts provisions for two 1-1/2`` , 2``, 2-1/2`` 3`` or 3-1/2`` conduits. This endwall also has knockout provisions for one 1/2`` or 3/4`` service ground conductor.



CTA-ID : 16041
Was this helpful?
What can we do to improve the information ?