Technical FAQs

Ask a Question

What type of hubs are used with the MPR33125 Meter-Pak?

This Meter-Paks` utility compartment will accept an A-L type hub (2`` through 4``) in the top endwall. Closing Plate ACPL is factory installed on the top endwall for a bottom cable entry application. The bottom endwall will accept two A-L type hubs (2`` through 4``).

CTA-ID : 16039
Was this helpful?
What can we do to improve the information ?