Technical FAQs

Ask a Question

Is the diameter of the hole (for the potentiometer shaft) in the 9001 KXB* potentiometer 3/8`` diameter ?

The potentiometer operator is used with a potentiometer with a shaft diameter of ``0.2475`` inches (approximately 1/4``) and 7/8`` long.


CTA-ID : 2000413
Was this helpful?
What can we do to improve the information ?