Technical FAQs

Ask a Question

What is the terminal size and temperature rating of a QO2100 ?

The terminals are rated for #12 - 2/0 75 deg. C aluminum or copper wire.


CTA-ID : 2000405
Was this helpful?
What can we do to improve the information ?