Technical FAQs

Ask a Question

Will the C125RB be rated 22,000 AIR interrupting rating by using the QOM1-VH breaker?

No. The C125RB is rated 10,000 AIR interrupting rating with the QOM1-VH breaker.


CTA-ID : 2000092
Was this helpful?
What can we do to improve the information ?